Hi,
What we understand is that you would like to implement the SPI protocol using GPIO's and not the module itself (due to the needs of the particular application).
This could be implemented if you follow the timing specifications for the device you want to communicate with (hold time, set-up time, etc...) and is inside the specifications for the platform. If everything is in line with what your device is asking, the device will not know if you are using GPIO's or the SPI module.
There is also the possibility to increase the number of bits to be sent (using the SPI module), but this number seems to be at 32bits MAX. I don't know how many bits you need to send continuously.
Please, let us know if the information helps you or not.