Update meta-alb recipes to enable HSE default support to make it convinient for users

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Update meta-alb recipes to enable HSE default support to make it convinient for users

511 Views
hittzt
Senior Contributor I

Hi there,

 

I noticed that, in BSP36, there is new bb files added for pkcs-hse demos and hse firmwares, it is simple than before.

But you can do more to update the bb files by adding HSE support in default, to make it more convinient for users . Because, even following the BSP user manual, adding the lines:

DISTRO_FEATURES:append = " hse"
NXP_FIRMWARE_LOCAL_DIR = "/path/to/firmware/folder"

in project conf/local.conf, then using the output sdcard image to boot the S32G board, take RDB3 as example, the board can not up, and will hang there:

NOTICE: Reset status: Power-On Reset
NOTICE: BL2: v2.5(release):bsp36.0-2.5
NOTICE: BL2: Built : 17:42:10, Mar 23 2023

And no more output.

This is because there needs more configures for atf, to make HSE related operations happy, but these steps should be done all manually as user manual shows. This is very unefficient and unfriendly for users. These related steps can be done in the related bb files automatically without so much effort.

So please consider to make it more simple and convinient to use for HSE feature.

 

Thanks,

Zhantao

0 Kudos
Reply
1 Reply

493 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback, we will forward this information to the internal team.

Have a great day.

0 Kudos
Reply