Unable to boot S32G-VNP-EVB3-S from SD card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to boot S32G-VNP-EVB3-S from SD card

811 Views
bhavanak
Contributor I

My company bought evaluation kit S32G-VNP-EVB3.  The processor is NXP S32G399A rev. 1.0. I followed the steps in the S32G3_LinuxBSP_31.0_user_manual ("write image" section of the document) to create a bootable sd card with the yocto .sdcard format.

I made sure the jumper settings are set currently as per S32G3_LinuxBSP_31.0_user_manual for qspi boot. ("boot from parallel RCON" section of the document). The boot did not go through and the following is what I see on the uart console. 

NOTICE: Reset status: Power-On Reset
PANIC at PC : 0x0000000034306740

Am I missing any step?

 

 

0 Kudos
Reply
1 Reply

627 Views
zhangmeng6
Contributor I

Has the problem been solved? I had the same problem starting with EMMC

0 Kudos
Reply