I need to connect "logitech hd pro webcam c920" to s32g-vnp-rdb2's usb port (I am using micro usb to type-A convertor). Board is detecting the camera as a USB device but not as USB camera. I cloned github.com/nxp-auto-linux/auto-yocto-bsp (bsp35.0) and enabled uvc and v4l2 in kernel and tried doing yocto build for "fsl-image-auto". But, after successful building, I am not finding "CONFIG_USB_VIDEO_CLASS" macro in kernel config file. Please let me know necessary steps to
Hello,@walking1
Thanks for the question.
I did some tests on our local RDB2 with BSP35, following are my comments for your reference:
First:
Device Drivers --->
Multimedia support --->
Media drivers --->
[*] Media USB Adapters --->
USB Video Class (UVC)
Then:
Device Drivers --->
[*] USB support --->
USB Gadget Support --->
[*] USB Webcam function
Then building the kernel images, after reboot, I could see the /dev/video0&1 device node. I tested it and found that an in-hand camera work fine.
Hope it helps.
Best Regards
Chenyin