U-Boot on S32G3 ping works only in one direction

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

U-Boot on S32G3 ping works only in one direction

ソリューションへジャンプ
128件の閲覧回数
yeshasyesodharan
Contributor I

I am working on an S32G3 board and able to ping from u-boot to the PC connected. 
However, it doesn't work the other way around.

Using pfe2 device
host 192.168.19.5 is alive
=> ping 192.168.19.5
Using pfe2 device
host 192.168.19.5 is alive
=> ping 192.168.19.5
Using pfe2 device
host 192.168.19.5 is alive
=> ping 192.168.19.5
Using pfe2 device
host 192.168.19.5 is alive
=> ping 192.168.19.5
Using pfe2 device
host 192.168.19.5 is alive
=> ping 192.168.19.5
Using pfe2 device
host 192.168.19.5 is alive
=> ping 192.168.19.5
Using pfe2 device
host 192.168.19.5 is alive


From the PC when I try to ping there is no response. 
The icmp packet was sent on the correct interface as observed using Wireshark. 

BSP-S32 

0 件の賞賛
1 解決策
98件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @yeshasyesodharan 

Thanks for the questions

It is correct for the results, u-boot only starts the network driver when it needs to use it (i.e. to send a ping). After it has finished the network driver is stopped. then Any traffic on the network will be ignored, as a result, no ICMP reply would be sent to the PC. 

 

Best Regards

Chenyin

元の投稿で解決策を見る

0 件の賞賛
2 返答(返信)
90件の閲覧回数
yeshasyesodharan
Contributor I

@chenyin_h 
Thanks for your response. Yes I also observed that u-boot responded to the ping requests received while u-boot was trying to ping the pc. It makes sense now. 

0 件の賞賛
99件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @yeshasyesodharan 

Thanks for the questions

It is correct for the results, u-boot only starts the network driver when it needs to use it (i.e. to send a ping). After it has finished the network driver is stopped. then Any traffic on the network will be ignored, as a result, no ICMP reply would be sent to the PC. 

 

Best Regards

Chenyin

0 件の賞賛