TSN support plan on GMAC for S32G platforms

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TSN support plan on GMAC for S32G platforms

862 Views
hittzt
Senior Contributor I

Hi experts,

 

I noticed that on S32G platform, there are TSN features supported as following:

1. GMAC

    Time Aware Shaper (IEEE 802.1Qbv), Time Synchronization (IEEE 802.1AS-Rev), and

    Frame Preemption (IEEE 802.1Qbu) for time-sensitive networking

2. PFE

     Supports 802.1AS-Rev and IEEE 1588 precision clock synchronization protocol

 

Especially, for GMAC, Qbu and Qbv features are supported, but it seems there is no related TSN configure application in userspace and TSN middle driver(like netlink driver) in kernel.

I wandar that, is there any plan or roadmap to add these components for TSN on S32G?

 

Thanks,

Zhantao

0 Kudos
Reply
1 Reply

844 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

At this moment it seems that only EST and PTP is going to be supported. There is no information as if there will be support for TSN under Linux userspace.

We could recommend sending this inquiry to your local NXP FAE for them to confirm this information.

Please, let us know.

0 Kudos
Reply