S32G3 bsp38 u-boot loads PFE firmware

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32G3 bsp38 u-boot loads PFE firmware

ソリューションへジャンプ
311件の閲覧回数
XD
Contributor I

Hi,

I am using BSP38 and have programmed the fip.s32-sdcard file to the eMMC. During the U-Boot boot process, I encountered a failure loading the PFE firmware, returning -1. According to the output of mtd list, the PFE firmware should be located at address 0x0000030a0000-0x000004000000.

I used Flashtool to program the s32g_pfe_class.fw file to address 0x30a0000 and set the pfengfw variable in the environment. Despite these steps, the PFE firmware still fails to load.

Could you provide guidance on the correct steps to ensure that U-Boot loads the PFE firmware properly?

Thanks,

XD

=> print pfengfw
pfengfw=0x30a0000
=> pfeng info   
Failed to get speed of XPCS for emac1_xpcs** No partition table - mmc 0 **
PFEng firmware file 'mmc@0:1:s32g_pfe_class.fw' loading failed: -1
PFE mode: enable
  emac0: sgmii emac1: sgmii emac2: rgmii
  fw: '0x30a0000' (from env)
=> 

 

0 件の賞賛
返信
1 解決策
270件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @XD 

Thanks for the post.

Yes, the uboot loads the PFE firmware from the partition 1.

Currently, from the BSP UM, only the full disk image that generated from Yocto build includes both FIP and PFE firmware.

 

BR

Chenyin

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
271件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @XD 

Thanks for the post.

Yes, the uboot loads the PFE firmware from the partition 1.

Currently, from the BSP UM, only the full disk image that generated from Yocto build includes both FIP and PFE firmware.

 

BR

Chenyin

0 件の賞賛
返信
262件の閲覧回数
XD
Contributor I

Hi Chenyin,

Thank you for your reply.

Do you have the partition table or the script to generate the image for reference?

Thanks,

XD

0 件の賞賛
返信
245件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @XD 

Thanks for the reply.

I've checked the related document, but seems currently no related script found, from my opinion, you may directly use the partation table of pre-built full images, then copy the PFE firmware to correct place.

Sorry for your inconvenience.

 

BR

Chenyin

0 件の賞賛
返信
279件の閲覧回数
XD
Contributor I

It appears that the eMMC lacks a partition, and U-Boot requires a FAT partition to load the firmware file.

Is there a way to generate a file that includes both the FIP and PFE firmware? Alternatively, is there another method to enable U-Boot to locate the firmware file?

Thanks,

XD

0 件の賞賛
返信