S32G SDK verson?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32G SDK verson?

跳至解决方案
1,622 次查看
Niupitang
Contributor III

After reinstalling S32G on the computer, opening the previous project prompts that the SDK version is inconsistent, but they are all SDK_S32_PA_11. Now the following error occurs when compiling. How to modify it?

1.png

 

0 项奖励
回复
1 解答
1,507 次查看
Niupitang
Contributor III

V2.1,I reinsta I hope it will not happen again in the futurelled the entire software and directly downloaded the latest installation package to solve this problem, LOL

在原帖中查看解决方案

0 项奖励
回复
8 回复数
1,613 次查看
Niupitang
Contributor III

The project CCU_V1_0_Z4_0 was created for Kinetis SDKSDK S32 PA 15 which is not installed in this product(repository SDK_S32_PA_15 not found).It is recommended to skip loading and install Kinetis SDK SDK_S32_PA_15 first (located in "[KSDK)/tools/eclipse_update"). If you continue loading,Processor Expert automatically converts configuration to use currently installed components.Such project might not work.

 

how to solve this problem?

0 项奖励
回复
1,579 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Would be possible that you tell us the product and the IDE that you are using?

 

0 项奖励
回复
1,508 次查看
Niupitang
Contributor III

V2.1,I reinsta I hope it will not happen again in the futurelled the entire software and directly downloaded the latest installation package to solve this problem, LOL

0 项奖励
回复
1,556 次查看
rehab_hassan
Contributor II

I have the same issue with s32 v2.1 and sdk 3.0.3 

i tried to open project from example for SBC 

I got this issue 

any solution?

 

0 项奖励
回复
1,535 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We understand you are working with S32 Design Studio IDE for ARM v2.1, which does not support S32G platform (which is this community main topic).

Could you please elaborate on which platform you are working with? (S32K1, KEA, etc...) for us to redirect this topic to the related community.

Please, let us know.

0 项奖励
回复
1,532 次查看
rehab_hassan
Contributor II

I am using S32 V2.1 for Power arch . for nxp5744p and I have the same error 

 

 

The project CCU_V1_0_Z4_0 was created for Kinetis SDKSDK S32 PA 15 which is not installed in this product(repository SDK_S32_PA_15 not found).It is recommended to skip loading and install Kinetis SDK SDK_S32_PA_15 first (located in "[KSDK)/tools/eclipse_update"). If you continue loading,Processor Expert automatically converts configuration to use currently installed components.Such project might not work.

 

 

0 项奖励
回复
501 次查看
mohammad_saad
Contributor I

@Daniel-Aguirre 
Can you please help with this issue.

0 项奖励
回复
1,214 次查看
hsuankac
Contributor I

Any updates on how to solve this issue? 

0 项奖励
回复