S32G Gold Box - AVB(openavnu)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32G Gold Box - AVB(openavnu)

2,879件の閲覧回数
minjun39
Contributor I

Hello 
I want start AVB in Gold box
so I was referring to openavnu 


https://github.com/Avnu/OpenAvnu

so I download zip file and I send that zip file to goldbox SD card by teraterm.

and I unzip the file and I tried cmake 
but it's not exist.
so I download cmake zip file too
and also upzip cmake file 
but there are no place in /dev/root

so I don't know how I get more place in root 

my sd card is 32GB

root@s32g399ardb3:/test/OpenAvnu-master# df -h
Filesystem Size Used Avail Use% Mounted on
/dev/root 353M 289M 42M 88% /
devtmpfs 1.6G 0 1.6G 0% /dev
tmpfs 1.7G 92K 1.7G 1% /run
tmpfs 1.7G 96K 1.7G 1% /var/volatile

Q1. Do you think It will work after root have more place?
Q2. How to get more place in root?

0 件の賞賛
返信
5 返答(返信)

2,850件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

On regards of OpenAvnu, we might not be the correct channel, since it does not seem to be directly supported by NXP, hence there is no documentation. We do apologize for the inconvenience.

As for increasing the size, we see there are the following threads that might proof useful:

Solved: Resize rootfs of Yocto image - NXP Community

Yocto - increase size of rootfs - Stack Overflow

This are not directly related to S32G, hence we cannot ensure the outcome might be the same. Again, we do apologize.

Please, let us know.

0 件の賞賛
返信

2,816件の閲覧回数
minjun39
Contributor I

Thanks for your answer but in my S32G Goldbox's Linux can't use 'sudo' 


'Auto Linux BSP 31.0 s32g399ardb3 ttyLF0'

how can I resize in this linux?


root@s32g399ardb3:~# df -h
Filesystem Size Used Avail Use% Mounted on
/dev/root 353M 289M 42M 88% /
devtmpfs 1.6G 0 1.6G 0% /dev
tmpfs 1.7G 92K 1.7G 1% /run
tmpfs 1.7G 104K 1.7G 1% /var/volatile

 

I want more size in /dev/root

0 件の賞賛
返信

2,796件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Under the Auto Linux for S32G, we understand that you already should have been a super-user, there is no need of sudo.

As for the specific information under S32G, we understand that there is no current guide for this. We do apologize.

We can recommend contacting your local NXP representative/FAE/DFAE (if any), to understand if under their channel there is any information available.

Again, we do apologize for the inconvenience.

Please, let us know.

0 件の賞賛
返信

2,726件の閲覧回数
minjun39
Contributor I

than can i use
'devtmpfs 1.6G 0 1.6G 0% /dev'
this part? How can i use this place? 

0 件の賞賛
返信

2,718件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

For the available documentation on this channel, we don't seem to find any specific mention of the devtmpfs command.

Can you share any logs on this regard?

We do apologize.

Please, let us know.

0 件の賞賛
返信