S32G ADC Maximum Rating

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G ADC Maximum Rating

536 Views
LukeChoi
Contributor I

Hi, 

I have a question of ADC(VREFH_ADC and VAD_INPUT).

What is the Max. VAD_INPUT value?   2.66V = VREFH_ADC(MAX 2.16V) + 0.5V?

Is VREFH_ADC of VAD_INPUT an instantaneous value? 2.3V = VREFH_ADC(1.8V)+0.5V?

LukeChoi_0-1662094447996.png

or Do I have to keep the operating condition of ADC?

2.17V = 1.92V+0.25 or 2.05V = 1.8V + 0.25 ?

LukeChoi_0-1662095565119.png

LukeChoi_1-1662095687988.png

 

 

0 Kudos
1 Reply

517 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

The VAD_INPUT value is directly related to VREFH_ADC. If, as an example, your design is using VREFH_ADC = 1.8V, then your Absolute MAX VAD_INPUT = VREFH_ADC + 0.5V = 1.8V + 0.5V = 2.3V.

As for the tables, It is always recommended to be under operating conditions (VAD_INPUT = VREFH_ADC + 0.25V). If you need to be under the absolute maximum ratings (VAD_INPUT = VREFH_ADC + 0.5V), there are several notes to take into account regarding the ADC inputs (S32G2 Data Sheet, Rev. 5, 05/2022, Table 3, notes 1,4,7,8). Below will be a summary for notes 1 & 4.

Note 1. This Absolute Maximum Ratings are stress ratings only, and functional operation at the maxima is not guaranteed.

Note 4. (Regarding VERFH_ADC)  Allowed 1.92V - 2.16V for 60 seconds cumulative over lifetime with no operating restrictions, 2.6 hours cumulative over lifetime with device in reset, at maximum Tj = 125 °C 

Hopefully this helps with your question.

 

0 Kudos