Hello,
I'm trying to import 'Mcu_Example_EBT_S32G274A_M7'or 'Adc_Example_EBT_S32G274A_M7' files from 'SW32G_RTD_4.4_3.0.3' to EB Tresos.It's OK.
But When I'm trying to import 'Pcie_Example_EBT_S32G274A_M7_001' files from 'SW32G_RTD_4.4_3.0.3' to EB Tresos. However, I always run into problems like XXX module is not installed.
After the check, the displayed module is 'XXX_TS_T40D11M30I2R0'.
Look at Any of the.xdm file in the Pcie example Config folder is value="ASPath:/TS_T40D11M30I2R0/xxx", while the xxx.xdm file in the other example Config folder is value="ASPath:/TS_T40D11M30I0R0/xxx".
How can this problem be solved?
Hi,
The difference in termination that you are seeing is related to the version of the specific plugin (RTD version, we might say).
It seems you are selecting a project with a different version of the plugin. If you have the specific version installed (it seems it is RTD v3.0.2), then you can go to:
"C:\nxp\S32DS.3.4\S32DS\software\PlatformSDK_S32XX_2022_03\SW32_RTD_4_4_3_0_2_D2203"
And look for the Pcie plugin (should be "Pcie_TS_T40D11M30I2R0"), then you copy the whole Pcie folder and paste it under:
"C:\EB\tresos\plugins"
In here, Tresos is searching for its plugins, could be that this specific plugin is not located in this folder.
Please, let us know if this information was helpful or not.