PEmicro can not step Debug with PFE driver demo on M7

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PEmicro can not step Debug with PFE driver demo on M7

308 次查看
longtengqiufeng1
Contributor III

Hi,

I want to enable PFE_MAC2 ethernet interface with LWIP and FreeRTOS on M7 core, so I download:

---SW32G_RTD_4.4_3.0.2_HF01_D2204.exe

--PFE-DRV_S32G_M7_MCAL_BETA_0.9.8.zip

--EB tresos 27.1.0

I refer to "Guide to enable PFE with LWIP based on RTD" document, follow it steps to modify the example demo lwip_s32g274a , it can run , but I cann't ping PFE_MAC2 ethernet interface.

When I step debug in line Eth_PFE_LLD_PlatformDrvPrepare(void) function , the console begin print many sentences like below picture :

longtengqiufeng1_0-1671688546744.png

then I press "suspend " or "terminate" button, the dialog boxes will be showed

longtengqiufeng1_1-1671688717797.pnglongtengqiufeng1_2-1671688734844.png

How can I solve this problem?

Thank you !!!!

 

0 项奖励
1 回复

258 次查看
MayanksPatel
NXP Employee
NXP Employee

Hi @longtengqiufeng1,

Can you please share TCP/IP Stack version?

We need to confirm the setup requirement is fulfilled by using RTD 4.4 3.0.2 and PFE 0.9.8 driver or not.

Have you used example for lwip_FreeRTOS_S32G274A_M7 Example which is available under TCP/IP Stack 1.0.3. This example directly compile on S32 Design studio.

 

Thanks,

Mayank s Patel

0 项奖励