Network error on s32g QNX7.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Network error on s32g QNX7.1

跳至解决方案
176 次查看
lewis123
Contributor II

Dear NXP,

 

I am running QNX7.1 on S32G-VNP-RDB2, but there are problems with the network.

The NIC dwc0 is identified after the system starts, I configured a valid ip for it.
But it can not ping other machines(return info: "ping: sendto: Host is down"), and no machine could ping the board.

Could you please suggest, is there any other work that needs to be done here.

Thank you for your support.

标记 (1)
0 项奖励
回复
1 解答
155 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Check with QNX since this works with the NXP BSP,

Regards

在原帖中查看解决方案

0 项奖励
回复
1 回复
156 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Check with QNX since this works with the NXP BSP,

Regards

0 项奖励
回复