Instalation SDK sja1110 in Ubuntu

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Instalation SDK sja1110 in Ubuntu

2,026 Views
cristianchacha
Contributor III

Hello

I have a issue with instalation of SDK sja1110 in linux. I achieved installed S32 design studio, but when I try to install the extension for use SDK sja1110 I didn't see any new package in S32DS Extensions and Updates.

I follow this procedure:
1.Install SDK sja1110
2. Download sja1110.update_3.5.230112.zip
3.Open S32DS, Windows > preferences > S32DS Extensions and Updates > Add and select previous file
4. Open Help > S32DS Extension and Updates

However I don't see any new "SJA1110 Package in the list"

 

How can manage that?

Is it available for ubuntu 20.04? because previously I add this in windows machine succesfully.

0 Kudos
Reply
7 Replies

1,934 Views
cristianchacha
Contributor III

actual status in S32Design studio is the following

cristianchacha_0-1694612021282.png

this message is still after several minutes , and I cannot instal sdk sja1110

 

0 Kudos
Reply

1,846 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

this is info I got from EA engineer showing WIN platform only fro SJA1110 SDK

PetrS_0-1694770343927.png

 

it is from S32 SDK for SJA1110 Quick Start Guide

BR, Petr

0 Kudos
Reply

1,841 Views
cristianchacha
Contributor III

Hi, coudl you provide me link to this documentation I not found for my side?

0 Kudos
Reply

1,831 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

Quick start guide is available in SDK install doc folder.

BR, Petr

0 Kudos
Reply

1,942 Views
cristianchacha
Contributor III

Hi,

yes it seems I need activate access to request update, do you know what sites I need ? when I desactivate site to updates I see next window , but obviously I don't have access to update

are you sure about RTDs online in linux?

how can I install sdk sja1110 ??

 

0 Kudos
Reply

1,980 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

so you have S32DS 3.5 successfully installed in Linux, only updatesite package content does not appear in S32DS Extension and Updates? Same steps works well on Windows. Are other updatesites functional?
What is step 1. I though development package and SDK is part of that update package.

But as far as I know RTDs online installation and so on are not supported in Linux for recent S32DS versions. 

BR, Petr

0 Kudos
Reply

1,623 Views
cristianchacha
Contributor III

Hello

Yes, I achieve install S32DS 3.5 in linux also SDK SJA1110 using Help > Installs New Software

I can build DEBUG_RAM and debug the program using P&EMicro, but I can't flash DEBUG_FLASH in non-volatile memory in SJA1110.

 

Is the objective of supporting Linux with sdk sja1110 for S32DS 3.5?

0 Kudos
Reply