How to communicate LLCE CAN to Host PC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to communicate LLCE CAN to Host PC

1,329 Views
Balavanth_1993
Contributor I

Hello Community,

I am working on S32G2 application gateway project, here our agenda is 

LLCE (CAN) IPC(M7)-IPC(A53)-GMAC

 i am testing with CAN communication for Core M7, for Flex CAN i am able to transmit and receive from PC to board vise-versa, but for LLCE CAN communication, getting passive error in CAN analyzer, so any body help me out on this issue.

Regards,

Balavanth

0 Kudos
3 Replies

1,291 Views
bpe
NXP Employee
NXP Employee

There are two software packages that can be of use for your project:

  • S32G2 Integration Reference Examples - this package includes a router application
    that does exactly what you want.
  • LLCE Standard Driver and Firmware - offers multiple driver use case examples
    showing how to properly initialize LLCE CAN and exchange data using it.

    Both packages are available through the Automotive Software Package Manager

Best Regards,
Platon

 

0 Kudos

1,218 Views
Balavanth_1993
Contributor I

Hello Platon,

while debugging process,i am getting following error for S32 debug probe test connection.

1.Can not access USB device.Please check if it is still connected.

regards,

Balavanth

0 Kudos

1,217 Views
Balavanth_1993
Contributor I

I have tried with System,laptop also, but still facing same issue.

0 Kudos