Failed to write SJA1110 flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Failed to write SJA1110 flash

320 Views
Junyu1
Contributor I

Hi guys,
I'm working with a S32G-VNP-RDB2 board.

Referring to the VNPRDBEEUG docs, I tried to download the firmware into the sja1110 flash with PEmicro(USB-ML-UNIVERSAL).

It seems that the debugger is not connecting with the chip

How to fix it?

s32ds.png

Thanks.

0 Kudos
3 Replies

294 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

just to be sure, do you have P&E multilink connected to right JTAG port (uP_DEBUG), set respective board's switches as mentioned in VNPRDBEEUG and power up board then before you start loading?

PetrS_0-1708948568575.png

BR, Petr

0 Kudos

288 Views
Junyu1
Contributor I

Hello Petr,

Thank you for your reply.

Yes, the same steps as in the documentation.Since SJA1110 works fine, is the debugger version too old to be burned?What should I do next?switch to a new USB-ML-UNIVERSAL-FX debugger?

Regards

0 Kudos

255 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

Multilink Universal Rev D should be an option too. 
What is a info displayed if you show Detail of error message?

BR, Petr

0 Kudos