FCCU fault EMCEM_FCCU_MTR_REPAIR_ERROR root cause confirm

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FCCU fault EMCEM_FCCU_MTR_REPAIR_ERROR root cause confirm

1,105 Views
Shenghao
Contributor III

Hi NXP,

Customer bring up M core only (BL doesn't load A core ATF image) and there is a FCCU fault triggered.

According to the flow chart from S32G RM, EMCEM_FCCU_MTR_REPAIR_ERROR occur before software invloving.

Does it mean there is a hardware design issue in customer's platform.

Or is there more document for FCCU fault clarify?

Shenghao_1-1683107472775.png

Thanks.

 

0 Kudos
Reply
5 Replies

1,057 Views
Shenghao
Contributor III

Hi Daniel,

They use S32G274A on their design with multicore booting by refering AN13750.

Below are their test summary, they check FCCU fault by observing register.

CASE1 - M core only (Boot loader doesn't load A core ATF image)
Result: EMCEM_FCCU_MTR_REPAIR_ERROR fault occur.

CASE2 - A+M core (A core boot up to uboot)
Result: EMCEM_FCCU_CM7_1_LOCKUP and EMCEM_FCCU_MTR_REPAIR_ERROR fault occur.

CASE3 - A+M core (A core boot up to kernel)
Result: EMCEM_FCCU_CM7_1_LOCKUP and EMCEM_FCCU_MTR_REPAIR_ERROR fault occur.
According to the attached (memory_repare_flow_chart) FXC found the EMCEM_FCCU_MTR_REPAIR_ERROR happens before SW involve.

The FCCU fault map has delviered before.

Thanks.

 

 

0 Kudos
Reply

1,039 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback.

We are not seeing the same behavior as your customer.

We have followed AN13750 and can successfully enable M7_0 under CASE1. We have used a blink example to verify the M7_0 execution after the bootloader.

EMCEM is related to SPD/SAF packages, which are not used under the AN13750.

Can you provide more information on how your customer is following AN13750?

If you require a private channel, you can open a ticket under the NXP online services.

Please, let us know.

0 Kudos
Reply

1,025 Views
Shenghao
Contributor III

Hi Daniel,

Apologies for missing to add the SPD version they use, it is SPD 1.9.0 HF01.

I'll try private channel to update it.

Thanks.

0 Kudos
Reply

1,018 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for the feedback.

Still, AN13750 does not talk about the usage/integration of SPD/SAF packages. Have they followed the guide without adding these packages and the result was as expected?

Please, let us know.

0 Kudos
Reply

1,094 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Which S32G variant is your customer using? Are they using an NXP reference board?

Also, we may not understand, is the Fault "EMCEM_FCCU_MTR_REPAIR_ERROR" happening to the customer? Or is it a supposition?  How does the customer know which FCCU fault is happening?

Is the customer using an NXP provided example? Which boot interface are they using (SD/QSPI or DEBUG)?

As for more information on regards of the Faults inside the S32G, depending on the variant, there is a *.xlsx file attached to the Reference Manual, which can be seen with a pdf reader that can look into the attached documents on a pdf:

DanielAguirre_0-1683149513781.png

Please, let us know.

0 Kudos
Reply