Eb tresos license issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Eb tresos license issue

1,633件の閲覧回数
Jitender1203
Contributor III

Hi,

we are working on CAN2ETH/ETH2CAN project, we took the NXP reference project from Golvip binaries. we are referring AN13423 document for this project.

In my desktop License is activated.

license eb.PNG

But Eb tresos is giving error like No license for Module.

license issue.PNG

we are facing this issue for every module.

タグ(1)
0 件の賞賛
6 返答(返信)

929件の閲覧回数
Abhijith_2000
Contributor I

Hi,

We are also facing the same license issues with Eb Tresos. Anyone, please help us solve this issue.

0 件の賞賛

1,537件の閲覧回数
gmocanu
NXP Employee
NXP Employee

Hello,

Could you try the evaluation license code found under the EB tresos Autocore product on nxp.com? That one should work for sure.

In the meantime, please make sure that the license code you use has all these features enabled:

gmocanu_0-1681108328732.png

 

Best regards,
George

 

0 件の賞賛

1,619件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Have you restarted Tresos Studio after the License has been updated?

We are seeing this behavior if we do not restart Tresos Studio once the license is updated.

Please, let us know.

0 件の賞賛

1,615件の閲覧回数
Jitender1203
Contributor III
Hi Daniel ,
Yeah, I have restarted Tresos studio after the license has been updated.
0 件の賞賛

1,610件の閲覧回数
asap
NXP Employee
NXP Employee

have you tried the step "update NXP plugins"?

take GoldVIP1.5.0 UM as an example, chapter 12.4, point 4.

"Replace the McalExt_TS_T40DxM1I0R0 plugin found in the
<EB_tresos_install_path>/plugins/ directory with the contents of
the McalExt_TS_T40DxM1I0R0.zip archive, which can be found in the
<GoldVIP_install_path>/configuration/can-gw/plugins directory.
The archive bundles the PFE and LLCE drivers referenced in Software prerequisites
chapter along with the required Real-time Drivers.
Note: EB tresos needs to be restarted after performing this change, in order to load
the newly installed plugins."

Albert
0 件の賞賛

1,586件の閲覧回数
Jitender1203
Contributor III

Hi ,
We already tried this step as per the Goldd VIP 1.0.5 manual , we copied the  McalExt_TS_T40DxM1I0R0 plugin (C:\Users\JK00868635\Desktop\nxp gold vip\GoldVIP-S32G2-1.5.0-binaries\configuration\can-gw\plugins\McalExt_TS_T40DxM1I0R0) & replace it with plugin found in Eb tresos plugin (McalExt_TS_T40DxM1I0R0).

But we are facing Same license issue. Can u plz help?

Regards
Jitender Kumar

0 件の賞賛