Could not repo s32g Yocto project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Could not repo s32g Yocto project

Jump to solution
1,618 Views
zhuliya
Contributor I

Dear NXP,

 

I am using s32g BSP 29.0 UM.  But When I tried to download the Yocto Project Environment following the manual and after repo sync, there are two errors as below:

meta-openembedded:
error: Unable to get pack file https://git.openembedded.org/meta-openembedded/objects/pack/pack-2016f3050542f84230130af7cbbe5452441...
GnuTLS recv error (-9): A TLS packet with unexpected length was received.
error: Unable to find d3d14d3fcca7fcde362cf0b31411dc4eea6d20aa under https://git.openembedded.org/meta-openembedded
Cannot obtain needed object d3d14d3fcca7fcde362cf0b31411dc4eea6d20aa
error: fetch failed.
error: Cannot fetch meta-openembedded from https://git.openembedded.org/meta-openembedded

Could you please help check this? Thanks a lot in advance.

0 Kudos
Reply
1 Solution
1,611 Views
bpe
NXP Employee
NXP Employee

This appears as an intermittent problem with the repository or an issue with
your local machine TLS. The suggestion here is to try it again later or use
another machine/network or reinstall the OS on it. The repo is working as expected
on my machines and there have been no similar reports.

Best Regards,
Platon

View solution in original post

0 Kudos
Reply
1 Reply
1,612 Views
bpe
NXP Employee
NXP Employee

This appears as an intermittent problem with the repository or an issue with
your local machine TLS. The suggestion here is to try it again later or use
another machine/network or reinstall the OS on it. The repo is working as expected
on my machines and there have been no similar reports.

Best Regards,
Platon

0 Kudos
Reply