Hi,
For what it is provided under the S32 Flash Tool User Guide, those 3 "CAN device name" are the ones provided.
Please, let us know.
Hi,
Under the S32G2 Reference manual, the following is told [Page 1341, S32G2 Reference Manual, Rev. 7, February 2023]:
"In Serial Boot mode, BootROM programs the HSE_H SWT for a 60-second timeout, then continuously polls for activity on any of the available interfaces:
•CAN
•UART
If no activity is detected, the timer expires and the core is reset. BootROM sequentially checks for activity on all available interfaces and selects the first serial interface that it identifies as active as the download interface."
If you want to use CAN for the serial download, then the LIN/UART interface should not be used, for it to detect activity on CAN and start using CAN.
Since this is related to the BootROM, you cannot disable one or the other.
Please, let us know.