Hi NXP Team,
I have installed some RTD2.00 of SBC,but I can't get the FS26 project on the S32K312EVB.I have seen the FS26 project of S32K344.
RTD verison is "SW32K3_FS26_R21-11_2.0.0_DS_updatesite_D2308" .
How should I do?
Expected reply.
解決済! 解決策の投稿を見る。
Hi Johnsy,
I checked FS26_4.4_1.0.0_RTM_D2209_Release_Notes.pdf \ FS26_4.4_1.0.0_CD01_D2208_Release_Notes.pdf \ FS26_4.4_1.0.0_CD02_D2303_Release_Notes.pdf, all were developed on S32K3X4EVB-Q257 board only. Although S32K312 is a supported derivative, you may need to refer to the S32K344 project to create a new S32K312 project and configure it yourself.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Johnsy,
I checked FS26_4.4_1.0.0_RTM_D2209_Release_Notes.pdf \ FS26_4.4_1.0.0_CD01_D2208_Release_Notes.pdf \ FS26_4.4_1.0.0_CD02_D2303_Release_Notes.pdf, all were developed on S32K3X4EVB-Q257 board only. Although S32K312 is a supported derivative, you may need to refer to the S32K344 project to create a new S32K312 project and configure it yourself.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------