S32K144 FreeRTOS_10 with MPU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 FreeRTOS_10 with MPU

1,001 Views
harish_g2
Contributor II

Hi All,

I ported FreeRTOS10 to s32k144 with the help of tutorials from muconeclipse on S32K144 https://dzone.com/articles/freertos-1001-with-nxp-s32-design-studio-2018r1

In this we can enable MPU from porcessor expert. After enabling this am getting errors as no functions defined for mpu wrappers. 

I wanted to know that anyoe ported FreeRTOS 10 with MPU support for S32K144.

Thanks in Advance...!
Harish G

0 Kudos
Reply
1 Reply

776 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Harish G

There is no need to ported the FreeRtos to version 10 because the latest SDK from S32DS already has this version, you need to update the software and it should be supported. regarding the MPU, there is a component MPU that you could use, does it work for your application?


Have a great day,
Jorge Alcala

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

0 Kudos
Reply