Hello NXP experts,
I'm using S32 Design Studio to configure CPU S32K142, package 64. It is strong and convenience : )
But I would like to have 2 questions
1st Question)
in Specification it notes that ADC0 has 16 external input channels
But when I configure ADC0 with external input channel 12 it always shows the error as ADC1 has 11 input only.
I think this is tool bug, how can I pass it to generate the ADC driver code correctly ?
2nd Question)
ADC1 of S32142-64 pins has 11 external input channels only. But look at the Peripheral Pins mapping
ADC1_SE9 is not available while ADC1_SE11 is connected to pin 53. In that case from Processor Expert, if I configure ADC1 with external input channel 11, it should be OK. But it again shows the error ?
How can I solve this problem ?
Kindly check
Thank you
Best regards,
Anh.Nguyen
Hello Jiri,
After changing the tool chain , I face with the new problem:
Build All error
Thank you alot
H.Anh
Hi Anh,
to clarify - you have an older project and you are trying it migrate into latest SDK because of package layout error in SDK you was using, am I correct? Or you start with new project from scratch with older SDK? What was your SDK version when you switch it into RTM 3.0?
If the second cause is yours - (started with new project) - the easy way how to migrate it into latest SDK is just start again and select RTM 3.0 in project wizard:
Jiri
Hello Jiri,
Bad luck I have an old project, toolchain is S32K142_SDK_gcc version 0.8.6
and I need to migrate to latest SDK
Which solution should be the best ?
Regards,
Anh
Hi,
may be someone from SDK team have better solution - but for me the only working way is create new empty project based on latest SDK, add all Processor Expert components (as on the old project), configure it again (based on values from old project) and copy source code into new project.
There is long time between these two versions and some components aren't compatible even for configuration store/restore.
Jiri
Hello Jiri,
Thank you a lot for your support : )
Anh
Hello again
I'm trying to replace SDK RTM 3.0.0 but it is impossible.
Do you know the reason is why ?
Thank you
Hi,
Yes, I'm using 64 pin package layout. What's your Toolchain? Latest SDK supports ARM Bare-Metal 32-bit target:
Jiri
Hello Jiri,
It is standard S32DS toolchain, should I change to ARM Bare-Metal ?
Hello Jiri,
Just confirm again, I'm using S32K142 64 pins package
If I configure ADC with S32K142 100 pins package there is no current errors
Hi,
please update your S32DS and use latest SDK version - RTM 3.0.0
https://community.nxp.com/docs/DOC-341068
In this version is ADC config working correctly:
Jiri
Hello Jiri,
This one should be the latest version right ? but I still meet the trouble.
Any other part of tool do I need to update ?
Thank you
Hello,
could you please specify which SDK version you use?
Regards,
Martin
Hello Martin,
I am using version 2018.R1
Is it too old ? Is there any update package available ?
Thank you