S32 Design Studio 3.3 和SDK的问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio 3.3 和SDK的问题

828 Views
turbozzg
Contributor II

安装完成S32 Design Studio 3.3之后显示S32K SDK为 4.0.0。整个安装过程没有报错,但是新建工程时,sdk选项中一个也没有,是空白的。 另外,下载了S32K RTM 4.0.1 发现不再是以前的zip文件,无法在S32 Design Studio中进行安装,它是一个独立的exe文件,安装以后,在S32 Design Studio也看不到,因此无法集成进去

Labels (1)
Tags (1)
0 Kudos
2 Replies

801 Views
turbozzg
Contributor II

Thanks, I am resolved

0 Kudos

810 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi turbozzg,

Have you try to select "NXP GCC 6.3 for Arm 32-bit Bare-Metal"?

S32DS Application Project.pngNXP GCC 6.3 for Arm 32-bit Bare-Metal.pngS32 SDK RTM 4.0.0.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------