I am trying to test the FlexCAN module using the S32 SDK 0.9.0 BETA for the MPC5744P. I have tried loading the example code, which on reception of a CAN message toggles the DEVKIT LEDs and also sends CAN messages when the switches are pressed. I am using a Vector VN1610 CAN-to-USB to communicate with the board when running, however, I seem to not be able to receive or send data to the board this way. On debug, I see that the program is stuck in the loop
while (FLEXCAN_DRV_GetTransferStatus(INST_CANCOM1, RX_MAILBOX) == STATUS_BUSY) { }
I have also monitored the signals from the CAN ports on the DEVKIT as well as the Vector VN1610 and I can read signals on the scope so I am unsure why the the transfer status cannot 'finish' i.e. the loop is infinite.
i have attached my set-up as well as the tests I have made on the oscilloscope.
解決済! 解決策の投稿を見る。
Hi,
I'd recommend to add terminating resistor 120 ohm between CAN_H and CAN_L terminals or populate SMD resistor 120 Ohm - R38 pads
Also please make sure you setup the CAN bus correctly on the PC side:
500kbps, 85% sampling point
Hope it helps.
Stan
Hi Chulue Zhong, Could you please share the example code which you used with the DEVKIT to transmit and receive CAN signals on the CAN0 port?
The example included with the S32 Design studio for MPC5744P DEVKIT sends CAN messages on CAN2 and I'm not sure how to monitor these using a Vector CAN case HW and Vector CANoe.
Thanks in advance.
The way I set up CAN was to use Processor Expert with the S32 SDK, which is an addon you can get from the S32 download page I believe. Then you can choose which FlexCAN module to use in a graphical interface and then add functionality by dragging and dropping code. Hence the final code set-up (FlexCAN only) for me was
in "main()":
// FlexCAN message struct for sending
flexcan_msgbuff_t send_buff;
send_buff.data[0] = 0;
send_buff.data[1] = 0xFF;
send_buff.data[2] = 0;
send_buff.data[3] = 0xFF;
send_buff.data[4] = 0;
send_buff.data[5] = 0xFF;
send_buff.data[6] = 0;
send_buff.data[7] = 0xFF;
send_buff.dataLen = 8; // data length
send_buff.msgId = 1; // Message ID
// FlexCAN Data Info
flexcan_data_info_t txInfo = {
.data_length = 8,
.is_remote = 0,
.msg_id_type = FLEXCAN_MSG_ID_STD,
};
// Initialize FlexCAN module
FLEXCAN_DRV_Init(INST_CANCOM1, &canCom1_State, &canCom1_InitConfig0);
// Configure Tx Message Buffer 0 to send CAN message
FLEXCAN_DRV_ConfigTxMb(INST_CANCOM1, 0, &txInfo, send_buff.msgId);
// Send the message
FLEXCAN_DRV_Send(INST_CANCOM1, 0, &txInfo, send_buff.msgId, &(send_buff.data));
while(1)
{
// Wait for transfer to complete
while (FLEXCAN_DRV_GetTransferStatus(INST_CANCOM1, 0) == STATUS_BUSY) {
//FLEXCAN_DRV_Send(INST_CANCOM1, 0, &txInfo, send_buff.msgId, &(send_buff.data));
counter++;
}
}
If you don't use the S32 SDK I think you can just replace CAN2 with CAN0 in the example code you saw, but you probably need to pay attention to the peripheral clocking for CAN0. On the DEVKIT, only CAN0 is connected to a proper CAN transceiver (MC33901WEF, see above) so with minimal set-up you would just need a 120-ohm resistor and some wires to connect to the Vector CAN peripherals.
Hi,
I'd recommend to add terminating resistor 120 ohm between CAN_H and CAN_L terminals or populate SMD resistor 120 Ohm - R38 pads
Also please make sure you setup the CAN bus correctly on the PC side:
500kbps, 85% sampling point
Hope it helps.
Stan
I do have an additional follow-up question, however. Are the values 500kbps and 85% sampling point dependent on the CAN transceiver (MC33901WEF) in the case of the DEVKIT? Also, the default sampling point was 87.5% actually, which worked.
Thanks very much, I now have the example code working. I thought initially that this resistor was already on the board.