Latest RTD (AR 4.7.0, SW 2.0.0) is missing the CSEc Driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Latest RTD (AR 4.7.0, SW 2.0.0) is missing the CSEc Driver

Jump to solution
164 Views
M_SCH
Contributor II

Hello,

I am migrating a project using the S32DS v3.5.12 relying on the  RTD with version

Autosar Version : 4.4.0
Autosar Revision : ASR_REL_4_4_REV_0000
SW Version : 1.0.0
Build Version : S32K1_RTD_1_0_0_HF01_D2109_ASR_REL_4_4_REV_0000_20210907

to the latest one with version

Autosar Version : 4.7.0
Autosar Revision : ASR_REL_4_7_REV_0000
SW Version : 2.0.0
Build Version : S32K1_RTD_2_0_0_P04_D2404_ASR_REL_4_7_REV_0000_20240417

I was checking the ConfigTool but realized that there is no CSEc driver available, which can be seen in the images below

M_SCH_0-1718202360087.png

ConfigTools (RTD, AR v4.4.0, SW 1.0.0)

 

M_SCH_1-1718202443656.png

ConfigTools (RTD, AR v4.7.0, SW 2.0.0)

I have checked the folder of both RTDs and verified that the folder below that features the required header files in the include folder

M_SCH_2-1718202576191.png

is missing in the new RTD folder structure (no Crypto_... folder)

M_SCH_3-1718202646317.png

  1. Can you point out what the issue is here?
    Have you removed the CSEc driver entirely or am I missing something?
    How can I proceed since my project is relying on this driver from the previous RTD.
  2. I have noticed that the SW32K1_S32M24x_RTD_R21-11_2.0.0_P04_D2404_ReleaseNotes.pdf specifically mentions the S32DS 3.5.4 version of the IDE. Since I use the 3.5.12 version I wonder if there might be some compatibility issues?

 

M_SCH

 

Labels (1)
Tags (1)
0 Kudos
1 Solution
139 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @M_SCH,

Sometimes patched releases do not include all drivers/modules. If there are missing drivers, another package is released, and this one should be used on top of the previous one.

I recommend using RTD 2.0.0 P02 or P03 for the crypto driver, since P04's release notes do not mention any changes to the crypto driver.

Best regards,
Julián

View solution in original post

2 Replies
140 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @M_SCH,

Sometimes patched releases do not include all drivers/modules. If there are missing drivers, another package is released, and this one should be used on top of the previous one.

I recommend using RTD 2.0.0 P02 or P03 for the crypto driver, since P04's release notes do not mention any changes to the crypto driver.

Best regards,
Julián

125 Views
M_SCH
Contributor II

Hello @Julián_AragónM,

 

Thank you for your suggestion.

Since I use a MCU from the S32K1xx family I have downloaded the zip folder

  • S32K1_S32M24x_RTD_R21-11_2.0.0_P03_CD01_D2312_DS_Updatesite.zip

and installed it offline inside the S32DS

  • S32DS --> Help --> Install New Software...
    • Add --> Archive
      • Select previously downloaded zip folder

M_SCH_0-1718373881816.png

I have installed the first two entries and then the Crypto driver appeared in the ConfigTool list and inside the RTD folder

M_SCH_1-1718374045896.png

 

Thanks again for your help!

 

Best regards,

 

M_SCH