Install S32SDK S32K1XX RTM 4.0.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Install S32SDK S32K1XX RTM 4.0.2

3,152件の閲覧回数
sergiverdaguerelausa
Contributor II

I am trying to install S32SDK S32K1XX RTM 4.0.2 but after install the downloaded exe the IDE doesn't recognise the installation. There are some guide describing the instalation throught .zip file but on downloads only are there the exe.

How to indicate to S32Design Studio to use my already installed S32SDK S32K1XX RTM 4.0.2 ?

 

Thank's!

Sergi

ラベル(1)
0 件の賞賛
返信
8 返答(返信)

3,130件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @sergiverdaguerelausa 

Which version of S32DS are you using?

This S32 SDK is delivered bundled in the S32 Design Studio v3.4. In this case, it’s already configured and ready to use.

 

B.R.

VaneB

0 件の賞賛
返信

2,484件の閲覧回数
DavidShu
Contributor II

My S32 Design Studio Version is v3.5, and my current S32SDK S32K1XX RTM Version is 4.0.1. how should i get v4.0.2? i could only see v4.0.1 in Design Studio update Center

0 件の賞賛
返信

3,095件の閲覧回数
sergiverdaguerelausa
Contributor II

Hi @VaneB

I am working with S32 Design Studio for S32 Platform 3.4 version.

On S32DS Extensions and Updates there is S32SDK S32K1XX RTM 4.0.3 but I want install 4.0.2.

 

Thank's for answer!

 

Sergi

0 件の賞賛
返信

3,084件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @sergiverdaguerelausa 

You should be able to find it at Help -> S32DS Extensions and Updates

VaneB_0-1679940908704.png

 

0 件の賞賛
返信

3,070件の閲覧回数
sergiverdaguerelausa
Contributor II

Hi,

As you can see on the screenshot I don't have 4.0.2, only the last one. 

sergiverdaguerelausa_0-1679986099468.png

Thank's,

0 件の賞賛
返信

3,051件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @sergiverdaguerelausa 

Download S32 Design Studio 3.4 S32K1xx Service Pack 1 (SW32K1_S32DS_3.4.1_D2106.zip) at My NXP Account -> Software Licensing and Support -> Software accounts and add it as an updated site.

VaneB_1-1680037506525.png

Please let me know if this works for you.

0 件の賞賛
返信

1,725件の閲覧回数
Eason_L
Contributor III

Hi VaneB,

After installing SW32K1_S32DS_3.4.1_D2106.zip, there's no RTM 4.0.1. How can I get RTM 4.0.1.

Eason_L_0-1701420285423.png

 

0 件の賞賛
返信

3,031件の閲覧回数
sergiverdaguerelausa
Contributor II

Hi @VaneB

It works!

Thank you,

 

Sergi

0 件の賞賛
返信