E_MEM_SERVICE_NOT_AVAIL macro undeclared (see Mem_43_INFLS.c) in latest RTD (AR: 4.7.0, SW: 2.0.0)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

E_MEM_SERVICE_NOT_AVAIL macro undeclared (see Mem_43_INFLS.c) in latest RTD (AR: 4.7.0, SW: 2.0.0)

Jump to solution
1,751 Views
M_SCH
Contributor III

Hello,

I am migrating an existing project based on the previous RTD (AR: 4.4.0, SW: 1.0.0) to the latest version (AR: 4.7.0, SW: 2.0.0 ). I am currently using the S32DS v3.5.12.

I have noticed that in the ConfigTools under the section MCAL the Fls driver is renamed/replaced by the Mem_43_INFLS, which should be the proper replacement, right?

When I attempt to build the application an error is thrown pointing at the generated C source file

  • RTD/src/Mem_43_INFLS.c at line 1013, 1093, 1445

with the statement

'E_MEM_SERVICE_NOT_AVAIL' undeclared (first use in this function) Mem_43_INFLS.c /my_project/RTD/src line 1013 C/C++ Problem

I have checked the BaseNXP driver documentation (RTD_BASE_UM.pdf) and noticed that the missing C macro is specified at page 151.

M_SCH_0-1718645629760.png

Then I checked the StandardTypes.h header file at line 141 but the macro -- as expected -- was missing.

M_SCH_1-1718645806041.png

 

Can you point out what the issue is and if I am missing something.

As a side node, I have found out that the macro is also defined in the MemAcc_GeneralTypes.h, which is not generated in my project right now.

M_SCH_2-1718645981316.png

 

One last thing: I have installed the following RTD package versions:

  • SW32K1_S32M24x_RTD_R21-11_2.0.0_P03_CD01_D2312_DS_Updatesite
  • SW32K1_S32M24x_RTD_R21-11_2.0.0_P04_D2404_DS_updatesite

 

Best regards,

 

M_SCH

Labels (1)
0 Kudos
Reply
1 Solution
1,531 Views
danielmartynek
NXP TechSupport
NXP TechSupport

You are right, it is missing in 2.0.0 P03, it is defined in 2.0.0 and 2.0.0 P04.

 

Regadrs,

Daniel

View solution in original post

0 Kudos
Reply
9 Replies
1,716 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @M_SCH,

I'm not able to reproduce the error.

When I create a new project from example:

Mem_43_INFLS_Example_S32K144

Once the default configuration is generated, I can see

danielmartynek_0-1718800560829.png

in

danielmartynek_1-1718800594930.png

 

Regards,

Daniel

 

 

0 Kudos
Reply
1,715 Views
M_SCH
Contributor III

Hello Daniel,

since I have installed the P03 and P04 RTD (AR: 4.7.0, SW: 2.0.0) package for the S32K1 series and the StandardTypes.h file which is included directly through the RTD installation folder at

  • S32DS.3.5\S32DS\software\PlatformSDK_S32K1_S32M24\RTD\BaseNXP_TS_T40D2M20I0R0\include

which shows the following version of the StandardTypes.h file:

M_SCH_0-1718801376330.png

 

Can you tell me how I can generate the code from the RTD P04 instead of the P03 package version again?

 

Best regards,

 

M_SCH

0 Kudos
Reply
1,699 Views
danielmartynek
NXP TechSupport
NXP TechSupport

It looks like an issue with the P04 installation.

I also updated to P04 from P03, but I have

S32K1_RTD_2_0_0_P04_D2404_ASR_REL_4_7_REV_0000_20240417

in the very same directory.

Maybe you can reinstall P04 in S32DS Extensions and Updates.

 

BR, Daniel

0 Kudos
Reply
1,694 Views
M_SCH
Contributor III

Hello,

I have uninstalled the RTD packages P03 and P04 of the latest version (AR: 4.7.0, SW: 2.0.0) and then installed P03 and then P04. Now all C source and header files indicate that they belong to P04 through their file header comment block but now I am missing again drivers such as the Crypto driver that is only available through P03 and both packages cannot coexist.

Can you confirm this on your side as well?

Best regards,

M_SCH

0 Kudos
Reply
1,683 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello M_SCH,

Yes, I can confirm that.

Refer to the release notes of the drivers, not all patches have this crypto driver.

 

 

0 Kudos
Reply
1,605 Views
M_SCH
Contributor III

Hello,

as you may recall I have installed the P03 package to make use of the Crypto Driver but at the same time I am missing the macro for the FLS driver that I mentioned in my original post and therefore cannot continue. Can you help me out? Do you have any suggestions?

Best regards

M_SCH

0 Kudos
Reply
1,552 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @M_SCH,

The P03 patch CD01 has the Crypto driver with CD quality status anyway.

danielmartynek_0-1719396255907.png

I would recommend migrating to the base version 2.0.0 at this point.

 

Regards,

Daniel

 

0 Kudos
Reply
1,543 Views
M_SCH
Contributor III

Hello Daniel,

I think you are missing the point. If you read my initial post you see that the C macro E_MEM_SERVICE_NOT_AVAIL is not available in the StandardTypes.h file in the P03 package. So I get errors using the FLS driver. That is why I posted this issue.

Can you confirm this issue on your side?

 

Best regards

 

M_SCH

0 Kudos
Reply
1,532 Views
danielmartynek
NXP TechSupport
NXP TechSupport

You are right, it is missing in 2.0.0 P03, it is defined in 2.0.0 and 2.0.0 P04.

 

Regadrs,

Daniel

0 Kudos
Reply