Hi,
I am trying to get an Irq from watch dog timeout but unable to do so. Could be please point out my error.
Below is the code snippet.
void watchdogtest()
{
/*Enable watch-dog*/
enable_irq (INT_SWT_0 - MAC57D54H_FIRST_USER_IRQ);
route_interrupt (INT_SWT_0 - MAC57D54H_FIRST_USER_IRQ, 0x03);
SWT_0.SR.R = 0x0000c520;
SWT_0.SR.R = 0x0000d928;
SWT_0.CR.B.WEN = 0;
SWT_0.TO.R = 0x500;
SWT_0.CR.B.ITR = 1;
SWT_0.CR.B.FRZ = 0;
SWT_0.CR.B.WEN = 1;
SWT_0.CR.B.SLK = 1;
uPrintf("In a While Loop...\n");
while(1); //
}
vector 122 is corresponds to SWT0
#define VECTOR_122 default_isr_test /*default_isr_test is dummy function to test an IRQ*/
clock SIRC is enabled .
and below is the register value corresponding to SWT0
Thanks in advance,
-Prashant
解決済! 解決策の投稿を見る。
Not sure what's wrong. I can see that also on computer connected to public net even if I'm not logged in. Is this link working on your side?
https://community.nxp.com/servlet/JiveServlet/download/816656-1-390566/halo-standby.zip
I will try to attach it again to this post with extension renamed from zip to aaa. Maybe it's caused by your firewall or something like that.
Access denied ..
Access to this place or content is restricted. If you think this is a mistake, please contact your administrator or the person who directed you here.
There is no attachment please check once again. And is it related to SIRC clk enable ? If yes then i have already enabled the clk as mentioned in previous mail . please check
Can you already see the attachment in my previous post? It seems that it is not visible immediately...
The example is related also to watchdog.
Lukas
No, it is not still visible. can we have other way please. waiting for your quick reply ..
Not sure what's wrong. I can see that also on computer connected to public net even if I'm not logged in. Is this link working on your side?
https://community.nxp.com/servlet/JiveServlet/download/816656-1-390566/halo-standby.zip
I will try to attach it again to this post with extension renamed from zip to aaa. Maybe it's caused by your firewall or something like that.
Yes i am able to download from below link. Thanks
https://community.nxp.com/servlet/JiveServlet/download/816656-1-390566/halo-standby.zip
BTW, if you are talking about enabling SIRC clk then we have already have below code at start up which is used to enable the SIRC.
/* Turn on FXOSC, SIRC and SXOSC - can integrate this into enable PLL step - leaving separate for now during testing */
MC_ME.DRUN_MC.R = 0x00130030;
MC_ME.MCTL.R = 0x30005AF0;
MC_ME.MCTL.R = 0x3000A50F;
let me know if it is different ..
-Prashant