USB Develepment

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Develepment

1,206 Views
无为无
Contributor III

Hi:

      I have a s32v234-sbc development board here. Now I connect an external camera to this development board using usb. How can I adjust this usb driver with this IDE( S32 DESIGN STUDIO FOR VISION v2.0 )。

Labels (1)
3 Replies

969 Views
mikedoidge
NXP Employee
NXP Employee

Hello,

How are you connecting this camera via USB? The USB port on the board is actually a USB to serial port for UART communication. However, you could connect a PCIe board with USB emulation support, but you would need to supply your own drivers for this.

Hope it helps,

Mike

969 Views
无为无
Contributor III

Hello,

      I have a miniPcie-to-usb3.0 module.But it is to hard for me, I'm compiling the kernel.

0 Kudos

969 Views
kaartic_sn
Contributor III

Hi 无为 无,

We are also trying to use a USB camera with the S32V234. It would be helpful if you could share the part number of the miniPCIe-to-USB3.0 module you are using? What is the chipset used in it? and which driver are you compiling to support the chipset?

0 Kudos