SW32G_RTD_4.4_4.0.1_D2302 installation fails

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SW32G_RTD_4.4_4.0.1_D2302 installation fails

Jump to solution
425 Views
ofer-bahar-guardknox
Contributor IV

Hi

Working in S32DS 3.5 with S32G2 and trying to add RTD 4.4 4.0.1 using the only available exe file SW32G_RTD_4.4_4.0.1_D2302 does not end but fails with the following error dialog 

oferbaharguardknox_0-1687982250456.png

Did this in two workstations, same result

Solution please 

 

 

0 Kudos
1 Solution
410 Views
ofer-bahar-guardknox
Contributor IV

Solved

It's the length of the installed directory, if exceeds 260 characters (windows limit) it fails

make it short

View solution in original post

Tags (1)
1 Reply
411 Views
ofer-bahar-guardknox
Contributor IV

Solved

It's the length of the installed directory, if exceeds 260 characters (windows limit) it fails

make it short

Tags (1)