S32K3 Sample Projekts (S32Kx4EVB-Q257)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K3 Sample Projekts (S32Kx4EVB-Q257)

跳至解决方案
2,066 次查看
JoDo
Contributor III

Hello, I have a S32Kx4EVB-Q257 Evalboard and I am trying to get the board working. I have installed the S32K3xx development package (SW32K3_S32DS_3.4.1_D2108.zip). However, I can't find any sample projects or use the configuration tool. Is there any additional software or packages that need to be installed?

I have installed:

S32 Design Studio 3.4
GDB Client for ARM Embedded Processors 9.2 Build 1701
NXP GCC for ARM Embedded Processors Build 1620
NXP GCC for ARM Embedded Processors Build 1649
S32 Design Studio Platform Package v 3.4.1
S32 Design Studio Platform Tools Package v 3.4.1
S32K3xx development package v3.4.1 EAR1
S32K3 FreeMaster Serial Communication driver v3.0

0 项奖励
回复
1 解答
2,049 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi JoDo,

You need to download and offline install S32K3 Real Time Drivers
DFAE should give you a link to download RTD and S32DS.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,050 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi JoDo,

You need to download and offline install S32K3 Real Time Drivers
DFAE should give you a link to download RTD and S32DS.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复