Hello
I developed all my code on the S32K144 EVAL board. However, the 64-pin version os the 144 MCU is not available in my region, so I have to port the entire code into S32K142. I tried just changing the processor in config. At first, it seems to be fine but I see two processors with the same name (Cpu:S32K142_64) under components->processors with one of the two is greyed. Also, RAM and FLASH appear under Generator_configurations with an "x" on RAM. After deleting the grey processor, if I double click on RAM, these errors popup:
"adc_pal.chg:undefined CPUfamily" and "adc_pal.chg:undefined CPUType".
Can someone explain to me what is happening? How do I fix this and port my code to that S32K142? I attached my project from S32K144 with this post.
Thank you,
Sri Harsha Pavuluri
已解决! 转到解答。
Hi,
you were using startup and linker files for S32K144. Here is step by step howto change package layout/family:
HOWTO: Change the CPU Derivative in an SDK-Based Application Project
In attachment is updated your project - unfortunately I have only S32K142 100 pin version and tested your project with this part (works okay - I can get into main). In the attached project is package switched back 64 pin version with fixed paths and so on - but untested with HW.
Jiri
Hi,
you are doing it right. The CPU change should be enough. For some reason - the ADC is complaining for CPU Family.
I removed ADC_PAL and add it again and fixed some missing paths. Basically - I renamed the project (by pressing F2 key when project name is active) - and S32DS fixed paths automatically but this is kind of workaround.
Anyway - the SDK team will probably add some additional info. In my opinion CPU change should work without any additional user steps.
In attachment is updated project - there is missing ADC settings (I left the default one) - just add it by yourself.
Jiri
Hi,
your program ends in exception for some reason (watchdog/clocking?). Are you able reach main function? Just try to figure out when the exception occurs. Invalid paths warning is okay - you can remove them from project settings. If it is possible you can share your project, I'll look at it.
Jiri
Hi,
you were using startup and linker files for S32K144. Here is step by step howto change package layout/family:
HOWTO: Change the CPU Derivative in an SDK-Based Application Project
In attachment is updated your project - unfortunately I have only S32K142 100 pin version and tested your project with this part (works okay - I can get into main). In the attached project is package switched back 64 pin version with fixed paths and so on - but untested with HW.
Jiri