S32DS3.4_Licence Issue_FC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS3.4_Licence Issue_FC

601件の閲覧回数
Fidel
Contributor IV

Dears,

         now I want to install S32DS on my PC,but I because I installed S32DS3.5 before, so the active code can be used anyone , I want to return it ,also failed ,details as below ,I also tried with a different account , the same issue, anyone can help me resolve that?  thanks a lot~

Fidel_0-1669166533898.png

 

 

0 件の賞賛
2 返答(返信)

584件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello Fidel,

The activation code you are using is tied to S32K3 Standard Software, it can be migrated forward to newer versions of S32DS, but not backward.

I recommend that you use the following links to entitle your account and receive S32DS version-specific licenses:

S32 Design Studio for S32 Platform v3.4

S32 Design Studio for S32 Platform v3.5

These links are also available in the download section of the S32 Design Studio for S32 Platform product page.

Best Regards,

Mike

0 件の賞賛

585件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

I checked your account and the license for S32DS v3.5 is returned. Do you have correct activation code for S32DS v3.4?

0 件の賞賛