[S32DS for Power v1.2] Error loading programming algorithm - load aborted.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[S32DS for Power v1.2] Error loading programming algorithm - load aborted.

2,657件の閲覧回数
tadashiyamagata
Contributor I

Hi

I tried using S32DS for Power v1.2 with DEVKIT-MPC5748G.

Select "New" - "New S32DS Project from Exsample" from the "File" menu and select "MPC5748G" - "hello" to create a project.
Select "Debug Configurations..." on the "Run" menu, set it appropriately on "Debugger" tab and press "Debug" button.

The following information appears in the Console and it can not write to the target.
-----------------------------------------------------------------------
Initializing.
MPC574xC Device detected.
Target has been RESET and is active.
CMD>CM C:\NXP\S32DS_Power_v1.2\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.7.2.201709281658\win32\gdi\P&E\nxp_mpc5748g_1x32x1520k_cflash.pcp

Initializing.
MPC574xC Device detected.
Initialized.

;version 1.05, 06/26/2017, Copyright P&E Microcomputer Systems, www.pemicro.com [5748G_6080k]

;device NXP, MPC5748G, 1x32x1520k, desc=CFlash

;begin_cs device=$00F90000, length=$005F0000, ram=$40000000

Loading programming algorithm ...
Error loading programming algorithm - load aborted.
Error occured during Flash programming.
-----------------------------------------------------------------------

I also tried S32DS for Power v1.1 in the same way.
In this version, no error occurred and writing to the target was possible.

Please advice on how to write to DEVKIT-MPC5748G with v1.2.

Regards,
Tadashi Yamagata

2 返答(返信)

2,451件の閲覧回数
tadashiyamagata
Contributor I

Dear Martin

Thank you for your reply.

It solved it by updating firmware of OpenSDA.

Thank you very much.


Regards,
Tadashi Yamagata

0 件の賞賛
返信

2,451件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

could you please try the procedure below:

1. Download OpenSDA Firmware (MSD & Debug) at link http://www.pemicro.com/opensda

Firmware Apps (.zip file).

Latest MSD & Debug applications. Updated June 28th, 2017.

 

2. You can find the update steps in file OpenSDA Firmware Update Instructions.pdf file.

 

3. Extract the DEBUG-OPENSDA-E200_Pemicro_v110.SDA file from the zip file.

 

4. Keep pressing the button SW3 (not SW1) , and connect the  DEVKIT-MPC5748G to the your PC using OPENSDA by USB cable.

 

5. You'll find a new BOOTLOADER driver on your PC, then copy the SDA file to the driver .

6. reset the DEVKIT-MPC5748G .

Please let me know, if it helps you.

Regards,

Martin