S32 Design Studio for Power Architecture; Mass Erase

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio for Power Architecture; Mass Erase

ソリューションへジャンプ
1,565件の閲覧回数
toby_lou
Contributor I

We are using a PEMicro Multilink Universal programmer/debugger for a MPC5748G based project.  In the S32 Design Studio for Power Architecture IDE, is there any way to have it perform a mass erase of flash before programming?

In a previous forum post (https://community.nxp.com/t5/S32-Design-Studio/S32-Design-Studio-Flash-Mass-erase/m-p/826471/highlig...), there is an screen shot of the S32 IDE that shows a mass erase option:

S32_MassEraseOption.jpg

This does not appear in S32 for PA.  Is there another way of performing that option?

0 件の賞賛
1 解決策
1,538件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

unfortunately this is not configurable in S32DS.

Regards,

Lukas

 

元の投稿で解決策を見る

0 件の賞賛
3 返答(返信)
1,542件の閲覧回数
toby_lou
Contributor I

You mentioned the standard erase where selected blocks can be erased. In the IDE, there does not seem to be any place in the "Debug Configuration/PEMicro Interface Settings" window where specific blocks can be selected for erase.  The programmer/debugger only seems to perform a "smart" erase, where only the flash blocks that have changed in the .elf file get erased. 

Where can selected blocks be specified?

0 件の賞賛
1,539件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

unfortunately this is not configurable in S32DS.

Regards,

Lukas

 

0 件の賞賛
1,557件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

S32K devices and MPC57xx devices have different flash modules. S32K supports mass erase function but there's nothing like that in MPC57xx devices. There's only standard erase where you can select blocks to be erased. So, there's no such option in S32 Design Studio.

Regards,

Lukas

 

0 件の賞賛