S32 Design Studio for Apple Mac

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio for Apple Mac

2,041件の閲覧回数
edgarmichel
Contributor II

Actually S32 Design Studio is available for Windows/Linux. Is there a port for Apple Mac available eg as Eclipse plugin?

ラベル(1)
2 返答(返信)

1,632件の閲覧回数
ajgar17374
Contributor I

I am using a MacBook Air 13 inch notebook and I am disappointed with the fact that S32 Design Studio IDE is not supported by MAC. You can go for byd studio as it is supported by Macbook as well as in your  iPad but don't try force installing or any other methods as once I tried and my MacBook Air  Won't Turn On and then I have to send it for repair  

0 件の賞賛

1,632件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

there is no version of S32DS for MAC. As a workaround you can use virtual machine (VMware, VirtualBOX...) on your Apple machine.

Jiri

0 件の賞賛