J-Link GDB Server failed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

J-Link GDB Server failed

1,490 次查看
Anjalipurushothaman
Contributor III

Please find the attched error message getting while hitting Run configuration.

There are different J-link open SDA-Generic firmwares? which one needeed to be installed?

hardware- s32k3x8EVB-Q289

IDE - S32ds3.5

0 项奖励
4 回复数

1,479 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

it looks that you have PE Micro OpenSDA debug probe, not the J-Link one. You can fix it by create new debug configuration for PE Micro OpenSDA. 

0 项奖励

1,443 次查看
Anjalipurushothaman
Contributor III
Inorder to create new configuration for PE Micro, that is not showing in the window(please refer the attached create,run configuration tab shared earlier).
0 项奖励

1,434 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

did you updated PE Micro package to latest version? 

jiri_kral_0-1687531457785.png

 

 

 

0 项奖励

1,429 次查看
Anjalipurushothaman
Contributor III
Yes, it is latest version. While using run configuration option (PE Micro debugger is not poping uo) wheras in the Debug tab it is showing.

Here I don't want to debug, I needto run the code into the target prcessor(Evaluation board)
0 项奖励