I cannot install any SW tool because the licenses were assigned to my old PC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I cannot install any SW tool because the licenses were assigned to my old PC

ソリューションへジャンプ
1,231件の閲覧回数
DavidMunozQuiroz
Contributor II

I cannot install all the SW tools because the license activation code is not valid for my new PC.

0 件の賞賛
返信
1 解決策
1,180件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @DavidMunozQuiroz , 

 

Please can you try offline activation method as per this page

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Activate-S32-Design-Studio/ta-p/...

 

Please let us know if that works. 

Thank you. Best regards. 

-Mehul Patel

元の投稿で解決策を見る

5 返答(返信)
1,196件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @DavidMunozQuiroz , 

 

As error message suggest, issue is because it failed to connect to license server. 

 

Please make sure that you have administrator right privileges while installing the S32DS. 

 

If the issue, persists please can you share the log of S32DS installation from

 C:\NXP\S32DS.3.4\_S32 Design Studio for S32 Platform 3.4_installation\Logs (or wherever your installation directory is located) 

 

Please follow the S32DS guide while installing S32DS: https://www.nxp.com/webapp/Download?colCode=S32DSIG 

Thank you. Kind regards. 

-Mehul Patel

0 件の賞賛
返信
1,186件の閲覧回数
DavidMunozQuiroz
Contributor II

Hi @Mehul_Patel_NXP,

I have make sure that I run the installer with administrator right privileges and it didn't work I am attaching the log file, possibly I need to get my offline license for my new PC because I don't know if being connected to my company network is blocking me the license validation, I can not disable the VPN just FYI,

  • Attached is the last installation try 
0 件の賞賛
返信
1,181件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @DavidMunozQuiroz , 

 

Please can you try offline activation method as per this page

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Activate-S32-Design-Studio/ta-p/...

 

Please let us know if that works. 

Thank you. Best regards. 

-Mehul Patel

1,176件の閲覧回数
DavidMunozQuiroz
Contributor II

It is getting installed now, this is an easy information overview for the next lucky person who fall in this problem:

-Start installation until license activation dialog is required
-Use your license listed in "https://nxp.flexnetoperations.com/control/frse/searchLicenses" for the product that you want to install.

-After setup the license and click OK it will appear online or offline activation dialog select offline

-This is a two steps request so first you save a request file "request.xml"

-Then you go to the offline license activation page in "https://nxp.flexnetoperations.com/control/frse/offlineActivation" load the "request.xml" then it will be downloaded an activation file "activation.xml"

The process could be confuse if you don't follow links at the beginning but it works for me thank you so much @Mehul_Patel_NXP 

0 件の賞賛
返信
1,155件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @DavidMunozQuiroz , 

 

You would require to go NXP website, login using account and go to Software Licensing and support and request for license for S32DS. 

Please follow this guide: 

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Activate-S32-Design-Studio/ta-p/....

 

Please let us know if there is issue while activation. 

 

Thank you. Best regards. 

 

- Mehul Patel

 

0 件の賞賛
返信