How to setup PFE driver in s32g274a

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to setup PFE driver in s32g274a

2,305件の閲覧回数
yihan_cheng
Contributor II

Hi 

I have downloaded the PFE Firmware file class_s32g.elf. But I don't know how to setup it.

In the user manuel said:

The fi rmware binary available on the target either in the le system or built into the driver depending on which driver is being used.

I copy class_s32g.elf to the root filesystem from my board in /lib/firmware/, however when i boot the EVB

PFEng firmware file 'mmc@0:1:pfe-s32g-class.fw' loading failed: -2

Thanks and Greeting

Yihan

0 件の賞賛
2 返答(返信)

2,171件の閲覧回数
athul_pk
Contributor I

Hello ,

I do have the same problem.

I have the bsp and yocto recipes for PFE . but from where I will get class_s32g.elf

Thanks in advance

0 件の賞賛

2,171件の閲覧回数
yihan_cheng
Contributor II

Hi,

I find the solution, there are bsp image with the PFE driver included. Beside it, you can use yocto to convert .elf to .bin

only the .bin files will work in linux image.

BR

Yihan Cheng

0 件の賞賛