I am writing TDP for S32 Design Studio for ARM Version 2018.R1 on IBM RTRT 8.0.1 on windows 10 I am Unable to access debugger through RTRT. I am using GHS (2017.14) compiler. So I need help to gain access to S32 IDE through RTRT.
Hello,
We do not provide support within the S32DS for ARM IDE for the IBM RTRT TDP. I see you are using Green Hills compiler, but which debugger are you using? If you used the GHS Eclipse Plugin, and created your S32DS application project using the new project wizard, then, as stated in the S32DS for ARM 2018.R1 release notes, only the Lauterbach debugger is supported. Perhaps you can contact Lauterbach for support for a debugger script for TDP.
Hope it helps,
Mike
Hi Mike,
Thanks for your reply I am using following configugration :
pegdbserver_console -device=NXP_S32K1xx_S32K146F1M0M11 -startserver -singlesession -serverport=7224 -gdbmiport=6224 -interface=USBMULTILINK -sp˜".
I am using :
Compiler: GHS 2017 .
Debugger: S32 Design Studio for ARM Version 2018.R1.
Hardware Device (Target Board): NXP_S32K1xx_S32K146F1M0M11
Interface=USBMULTILINK -sp˜".
Please provide reference (TDP -debugging script ) so that I can interface IBM RTRT for TDP with S32 Design Studio for ARM Version 2018.R1.
Regards
Abhishek Mohanty