i tried to use full chip simulation with mc9s12xdg128,but there is a error when i make.
the error is L1822,symbol delatms in file D:\program\project_3_Data\standard\objectcode\main.c.o is undefined;
i first use CW for HS12 ,please help me.think you!
Hello
This message indicates that in file main.c you are using a symbol called delatms which is not defined anywhere.
Most probably you did forget either to add a library or a source file to your project.
If delatms is a function you need an implementation of this function.
If delatms is a variable or constant you need a definition for the variable.
That is all I can say from the message alone.
CrasyCat