using the CW MCU v11.1 development platform, the PE tool failed to burn

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

using the CW MCU v11.1 development platform, the PE tool failed to burn

678 Views
zhouqicheng
Contributor I

Hello, using the CW MCU v11.1 development platform, the PE tool failed to burn and the circuit board has 5V. The following interface always pops up. How can I solve this problem

0 Kudos
Reply
1 Reply

664 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

if you have a problem with P&E USB Multilink Universal (firmware update), then you should ask P&E support. www.pemicro.com

However.....

I suppose you use Windows 10.

Did it work before?

Have you plugged the cable in correct orientation into the board?

Are you using your own board or an EVB?

 

Best regards,

Ladislav

0 Kudos
Reply