target MCU has no clock or wrong BDMclock speed is used of derivative is unsecured

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

target MCU has no clock or wrong BDMclock speed is used of derivative is unsecured

1,569 Views
parvathipradeep
Contributor I

Sometime while programming MC9S12DG128CPVE with universal multilink programmer I get the following error ( screen shot is attached): "Communication with target failed : The target MCU has no clock or wrong BDMclock speed is used of derivative is unsecured" Once programmer recovered from this state on its own. But how do I recover from this state now ?

Tags (1)
1 Reply

1,017 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi Parvathi Pradeep,

This error can be caused by a variety of reasons. Under the similar cases on the below links are described possible reasons for the error.
Did you look at the below links and checked possibilities which can cause your issue? 

Communication with the target failed:  The target MCU has no clock or wrong BDM clock speed is used ... 

 

 

Best regards,

Diana