mc9s12g128 Write Eeprom

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mc9s12g128 Write Eeprom

601 Views
张华荣
Contributor II

When I use BDM debug the MCU,the eeprom can be written,but when I disconnect

the BDM and restart the MCU,the eeprom can not be written.I do not know

why?Please help me,thanks.

 

The .prm is:

/* This is a linker parameter file for the MC9S12G128 */

NAMES END /* CodeWarrior will pass all the needed files to the linker by command line. But here you may add your own files too. */

 

SEGMENTS  /* Here all RAM/ROM areas of the device are listed. Used in PLACEMENT below. */

 

/* Register space  */

/*    IO_SEG        = PAGED         0x0000 TO   0x03FF; intentionally not defined */

 

/* RAM */

      RAM           = READ_WRITE    0x2000 TO   0x3FFF;

 

/* D-Flash */

     DFLASH        = READ_WRITE   0x000400 TO 0x0013FF;

Labels (1)
0 Kudos
1 Reply

372 Views
iggi
NXP Employee
NXP Employee

The .prm file is as usual.

The most probably there is a problem with a register which is Write Once in Normal mode (no BDM connection).

Here is the S12G Examples Pack and there is one demonstrating EEPROM E/W routines. The project is made for S12GN32 derivative, but the main.c source code can be used on S12G128 as well. Of course, the difference is the EEPROM size and so the end memory address.

Hope it helps.

regards,

iggi

0 Kudos