mc9s12dg128 cfu 3L40K

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mc9s12dg128 cfu 3L40K

585 Views
honda_repsol
Contributor I

good afternoon looking for replacement MC9S12DG128 CFU 3L40K . could you pls help me? thx in advance

Tags (1)
0 Kudos
1 Reply

414 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi Johny,

Unfortunately, there is no direct replacement.

Depend on your application requirements and peripherals which are relevant for you.

Very useful and well-arranged document about automotive devices it can be also helpful for choosing the right device. See 16-bit S12(X) MCUs or 16-bit S12 MagniV MCUs.

http://pdf1.solecsy.com/26/78c49d0c-741a-43be-a512-9ca142bc5ffc.pdf 

The products which can be found on the below link are available for a minimum of 10 years from product launch

Product Longevity|NXP 

 

The MC9S12DG128CFUE with 5L40K mask set is still active, but that device is not in longevity program.

MC9S12DG128CFUE Product Information|NXP 

You can look at  

S12XD devices are still active, but that devices are not in longevity program.

S12XD MCUs|16-Bit Microcontroller|NXP 

S12XE:

S12XE MCUs|16-Bit Microcontroller|NXP 

or S12G:

S12G Optimized MCU |16-bit MCUs|NXP 

In the attachment, you can see the application notes about compatibility. The devices from the S12XE family like S12G, etc. are not the replacement, for example, the difference is in the memory map.

I hope the information helps.

Best regards,

Diana

0 Kudos