Hi I checked floating point program but its showing error
#include <hidef.h> /* for EnableInterrupts macro */
#include "derivative.h" /* include peripheral declarations */
#include "math.h"
void main(void) {
EnableInterrupts;
/* include your code here */
float a=4.5;
float b=5.5;
float c;
c=a+b;
for(;;) {
__RESET_WATCHDOG(); /* feeds the dog */
} /* loop forever */
/* please make sure that you never leave main */
}
how to correct this code to check floating point operations?
i need to do natural log calculations also for below mentioned expression will it possible ?
#define A1 -13.4088568
#define B1 4547.9615
#define C1 -176965.92
#define D1 3861154
#define R25 10000 //10KOHM
#define R1 1000 // 1KOHM
//To Find Rt
Rt = {(4096/ADC)-1}*R1
//and To Find Temprature T
RtR25 =Rt/R25
result1 = log(Rt);
result2 = log(Rt)*log(Rt);
result3 = log(Rt)*log(Rt)*log(Rt);
//TEMP_KELVIN =1/(A1+B1+ln[Rt/R25]+C1ln2[Rt/R25]+D1ln3[Rt/R25]) (ln-natural log)
TEMP_KELVIN =1/(A1+B1+result1+(C1*result2)+(D1*result3))
TEMP_DEGREE=TEMP_KELVIN+273
Hi Sathish,
Please add the right ansi library.
Under Settings + S12Z Linker + Input, the Libraries (see picture above) you must change the lib file used.
\CW MCU v10.6.4\MCU\S12lisa_Support\s12lisac
The readme.txt will provide more info to select the right lib file.
I hope it helps you.
Have a great day,
RadekS
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Sathish,
When you create new project, you could select type of Float/Double type implementation.
Appropriate ANSI IEEE-754 Floating Point Library will be linked with your project.
I hope it helps you.
Have a great day,
RadekS
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------