Why the Hall current sensor signal can not be amplified by Current sense amplifier AMP0?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why the Hall current sensor signal can not be amplified by Current sense amplifier AMP0?

1,536件の閲覧回数
maxxu
Contributor IV

Hi

   I design the motor driver using mc9s12zvm。

   I use the hall current Sense ACS758 to sample the current,Output voltage, 2.5V.

   To use over current comparator internally,I enabled and connected amp0.

    When the input signal is 2.5V DC, the voltage of AMPP [0] pin is 1.25V, which is correct. However, AMPN [0] and AMP [0] can't output normally. They are high-frequency oscillation waveforms, similar to sine wave, which seems to be self-excited oscillation,
This circuit I use in other physical op amp amplifier (such as lm358) processing waveform is normal

无标题1.jpg

I'd like to ask you some questions


1. Is the Current sense amplifier inside the chip different from the independent operational amplifier
2. Can Hall current sensor be used in internal Current sense amplifier without low resistance sampling resistor

3. How to use Current sense amplifier to realize the function of amplification factor 1

  

0 件の賞賛
3 返答(返信)

774件の閲覧回数
Oliviahyang
Contributor I

Hi, so you get any answers? I also want to do the current sensor amplifier simulation, and couldn't find the amplifier simulation model.

Thank you so much.

0 件の賞賛

1,479件の閲覧回数
maxxu
Contributor IV

It's really a question. Can someone help me

0 件の賞賛

1,509件の閲覧回数
maxxu
Contributor IV

why?

0 件の賞賛