Dear friend,
I had use Automotive part# S9S12G48F0MLF,
1. Use CyclonePro to program
2. Add security function in CyclonePro
3. But want to reprogram and unsecurity will fail.
4. If use PC & Codewarrior 5.1 & U-Multilink can to reprogram and unsecurity.
Pleas help check reprogram and unsecurity in Cyclone Pro (S9S12G48F0MLF).
Thanks a lot.
Solved! Go to Solution.
Johnny,
From the screen shot you supplied, I see that in the pop-up menu under the Security Settings, you have a "Generic" device selected. This setting is only for the S12 0.25u devices. For the S12G and S12P device family, which are 0.18u devices, you must select "Pxxx" from the pop-up menu. That should solve your problem.
Best Regards,
Gordon
Johnny,
From the screen shot you supplied, I see that in the pop-up menu under the Security Settings, you have a "Generic" device selected. This setting is only for the S12 0.25u devices. For the S12G and S12P device family, which are 0.18u devices, you must select "Pxxx" from the pop-up menu. That should solve your problem.
Best Regards,
Gordon
Dear Gordon,
Your suggest can fix this issue.
Thanks a lot for your support.