SPI problem (MC9S12P and MMA7455L)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPI problem (MC9S12P and MMA7455L)

407 次查看
Mishup
Contributor I

Hi everyone,

 

I'm trying to communicate uC and accelerometer, but I am not able to.This is how I configure SPI using Device Initialization:

 

  /* ### Init_SPI init code */  /* SPICR1: SPIE=0,SPE=0,SPTIE=0,MSTR=0,CPOL=0,CPHA=0,SSOE=0,LSBFE=0 */  SPICR1 = 0U;                         /* Disable the SPI module and clearing flags in SPISR register */  /* SPICR2: XFRW=0,MODFEN=0,BIDIROE=0,SPISWAI=0,SPC0=0 */  SPICR2 = 0U;                                        /* SPIBR: SPPR2=0,SPPR1=0,SPPR0=0,SPR2=0,SPR1=0,SPR0=0 */  SPIBR = 0U;                                        /* SPICR1: SPIE=0,SPE=1,SPTIE=0,MSTR=1,CPOL=0,CPHA=0,SSOE=0,LSBFE=0 */  SPICR1 = 80U;

 And this is example of writing to SPI slave device:

void acc_write_reg(byte reg, byte val)    {       byte x;      ACC_SPI_CS =0;
 while (!SPISR_SPIF); //wait for transmission completex=SPIDRL; //dummy readSPIDRL= val ;while (!SPISR_SPIF); //wait for transmission completex=SPIDRL;    ACC_SPI_CS = 1;     }

But while debbuging I saw that this part:

 

       x =((reg << 1) | 0x80);        SPIDR =  x;

 resultes with 0xFF SPIDR value. And no matter what I put there, it doesn't change. What do I do wrong?

 

I'll be grateful for any help!

 

Michael

标签 (1)
0 项奖励
0 回复数